October 02, 2024

Share:

Introduction

Developing intelligent, high-performance vision systems is a lengthy and extensive process typically taking around six months. Improving time-to-market for these vision systems while optimizing engineering resources is critical to the success of these complex vision designs. To aid in the camera development process, onsemi has developed a reference module ecosystem for our image sensors called Premier Reference Image Sensor Modules (PRISM).

In this blog you will learn about the PRISM ecosystem, its benefits and how to get started with PRISM.


PRISM & its Benefits

PRISM is a pre-optimized sub-system solution developed with onsemi’s industrial and commercial image sensors. Additionally, any new sensors introduced from onsemi will include PRISM as a part of its standard deliverables. The modules, combined with hardware adapters and ecosystem partner development kits, can be used for prototyping purposes and shorten the prototype design process for faster time to market.


Figure 1: Full Portfolio of PRISM Modules


A typical vision system consists of many elements including optics (lens), image sensor, sensor interface, image signal processor and application software or artificial intelligent (AI). The lens and sensor need to match perfectly within a proper form factor to maintain the quality of the input image. Any slight mismatch can result in artifacts that impact the overall system performance. 

Alongside the modules, onsemi provides supporting material explaining how to further develop PRISM into a mass production design. Validation reports are provided under NDA for sensor’s performance baseline. A standardized interface of PRISM adaptor is also provided to connect PRISM to major AP/SoC platforms.

Figure 2 below provides a high-level outline of the PRISM ecosystem design stages.

Figure 2: PRISM Ecosystem


Premier Reference Image Sensor Modules

Below, is a complete list of onsemi image sensor modules supported by the PRISM ecosystem.

  • PRISM1M-AR2020CSSC130110-GEVB: This high-resolution 20 MP module is designed, built and validated with including video conferencing endpoints, AR/VR headsets and more. It’s innovative SmartROI feature delivers 20 MP performance without the needed bandwidth. The sensor drivers and base tuning are available with major SoC platforms.
  • PRISM1M-AR0830CSSC130110-GEVB: This 8 MP sensor is designed, built and validated with lowest possible power consumption, impeccable imaging performance, and system saving features for applications including doorbell cameras, smart access and more. Its wake on motion feature allows for the lowest power consumption among comparable sensors in the industry.
  • PRISM1M-ARX383CSSM130110-GEVB: Featuring the ARX383, this tiny 0.3 MP global shutter module is designed, built and validated with performance baseline for size-constrained applications including handheld QR barcode scanner, autonomous mobility and more.
  • PRISM1M-AR0145CSSM130110-GEVB: This 1 MP global shutter module is designed, built and validated with performance baseline for applications including barcode reader, autonomous mobile robots and more.
  • PRISM1M-AR0235CSSM130110-GEVB: Featuring the AR0235 image sensor, this 2 MP global shutter module is designed, built and validated with performance baseline for applications including barcode reader, autonomous mobile robots and more.
  • PRISM1M-AR0822NPSC130110-GEVB: This 8MP module is designed, built and validated with performance baseline for applications that requires a HDR built in sensor especially in multiple camera system. Such multiple camera system usually consumes data transmission bandwidth between the sensor and ISP/SoC. Whether it is a single or multi-camera design, the AR0822 helps optimize HDR and reduce much of the bandwidth burden with its on-board eHDR.


Getting Started with PRISM

Expediate your prototype development process with our innovative image sensor modules and surrounding ecosystem tools. To learn more about PRISM, download our whitepaper or contact sales.


Additional resources


Featured

Machine Vision

With the most image sensor offerings from VGA up to 45 MP, onsemi has the right sensor for your machine vision application.

Our intelligent sensing solutions are developed with decades of imaging expertise and proprietary pixel design processes, delivering the best quality and efficient image capture. Offering unique features tailored to the machine vision market, onsemi image sensor families provide the industry’s best global shutter efficiency and frame rates exceeding modern camera needs. These features, alongside system components designed specifically for our sensors, allow you to design reliable inspection cameras that capture high-quality images without blurriness.

Security and Surveillance Cameras

onsemi provides a diverse portfolio of image sensors with innovative features and capabilities by delivering excellent image quality at low power consumption. This portfolio addresses a wide variety of applications such as biometric scanners, facial recognition systems, state-of-the-art surveillance cameras, and security & safety systems.

Our image sensors are built to overcome challenging lighting conditions by offering wide dynamic range and low-light performance to give your device the best results in any circumstance. onsemi offers a comprehensive image sensor product portfolio that supports low power consumption. Our best-in-class image sensor development ecosystem software saves design time and enables short time to market (TTM).