March 17, 2025

Share:

Industrial machines showing the image sensor

One secret behind the success of modern industrial automation is the power of 3D vision. Traditional 2D sensors can only provide flat images, creating limitations in their effectiveness in applications like device inspection. They can read a barcode which may contain the items’ dimensions but cannot independently gauge true shape and size, or any potential dents, defects or irregularities. Furthermore, 2D readings are at the mercy of lighting conditions, which may obfuscate or distort important areas of interest.

A breakthrough to these constraints can be done with depth sensing, processing the Z-axis in 3D, much like human vision. Now, depth cameras can tell the fullness of an object, perform precise inspections on devices, and even detect subtle facial features for applications such as access control. Thanks to these capabilities, 3D vision is a game-changer across industries - from defense and aerospace to medical, automotive and consumer tech. Whether it's obstacle detection, facial recognition, self-driving or robotic assistants, depth sensing is the key to modern industrial automation.

Depth sensing, regardless of type, relies on active or passive visual illumination. Depth sensing based on passive illumination typically requires highly calibrated stereo sensors and parallax, very similar to the human eye. Active sensing uses an emitted light beam towards their targets and uses the reflected energy to determine depth. This requires an energy emitter, but offers advantages like penetrating clouds/smoke, 24/7 operation and more deterministic operation.

There are several active illumination techniques: direct time-of-flight (dToF), indirect time-of-flight (iToF), structured light and active stereo. Indirect time-of-flight uses phase shift between the transmitted and received signals to calculate distance - it's very accurate and the illumination hardware is simple.

In this blog you will learn about onsemi’s newest family addition, Hypelux ID which has made significant advances in iToF technology and how these advancements can be utilized to improve depth sensing in current industrial and commercial applications.


Existing iToF Technology Constraints Reduce Widespread Adoption

iToF sensing lies at the heart of many applications. One such popular application is face recognition as seen on various smartphones.  However this access control feature can only function at close range. Other applications that use iToF include machine vision (MV), robotics, augmented reality/virtual reality (AR/VR), biometrics and patient monitoring. Currently these applications are restricted to indoor use at close range (< 5m) with stationary objects that do not require high resolution. Several challenges restrict the potential scope of iToF technology. Among these are motion, the overhead and complexity of the hardware and data processing architecture and the need for meticulous calibration.

These significant hurdles either force engineers to implement complex 3D and expensive solutions to obtain depth, or simply to not acquire depth information at all. With remarkable innovations, onsemi introduces the Hyperlux ID family that enables the benefits of iToF without previously noted restrictions. Hyperlux ID’s iToF implementation can now enable a more widespread adoption of this important technology.


Detailing the Hyperlux ID Advances

onsemi’s Hyperlux ID sensing family initially consists of two 1.2 megapixels (MP) iToF products, the AF0130 and AF0131. This family provides advanced sensor performance and development in four critical areas:

1. Receiving reliable depth information with moving objects

2 Achieving optimal resolution/depth distance with high accuracy

3. Reducing cost and size

4. Decreasing calibration time


Each of the aforementioned areas and improvements are further detailed.


Reducing Motion Artifacts

To enable more widespread adoption, iToF sensors need to function well with moving objects, so they can produce accurate results without motion. As mentioned, iToF sensing relies on light reflections using four or more different phases to calculate depth.  Nearly all existing iToF sensing solutions in the marketplace do not capture and process these phases simultaneously which provide issues with moving objects. Designed with a unique proprietary integration and readout structure, the Hyperlux ID depth sensor uses global shutter with on-chip storage and real-time processing to enable fast-moving object capture applications such as conveyor belt operation, robot arms, surveillance, collision avoidance, gesture detection and more.


iToF Applications in Warehouse


Increased Resolution = Higher Accuracy and Expanded Depth

Most iToF sensors on the market today have only VGA resolution, which hinders their accuracy, and in turn, limits their applications. One reason VGA is more prevalent is due to the complex phase capture and data intensive processing mentioned prior.  In contrast, the Hyperlux ID sensors are designed with 1.2 MP resolution (1280x960) using a high performance 3.5 µm back-side illumination (BSI) pixel. As a byproduct of its increased resolution over VGA, the Hyperlux ID sensor offers the additional critical advantage of expanded range depth. Additionally, at closer distances high-precision accuracy is provided and wider-angle optics can be used.

With higher resolution, the Hyperlux ID sensors also delivers improved quantum efficiency and reduced depth jitter. Taken together, these enhancements mean new applications for iToF sensors where high resolution and expanded depth are paramount, such as gesture recognition, quality control/inspection and access control.


Existing  iToF solutions (left) vs onsemi’s new advanced Hyperlux ID iToF (right)
Existing iToF solutions (left) vs onsemi’s new advanced Hyperlux ID iToF (right)


Longer Range

As a byproduct of increased resolution, the Hyperlux ID depth sensor can measure depth over a much greater range compared to other iToF sensors currently available. While current iToF offerings have an indoor range of less than 10 meters, the Hyperlux ID iToF sensor family can reach up to 30 meters. The usage of a high-performance global shutter pixel enables a full sensor array to closely align to active infrared lighting, which in turn limits noise provided from other infrared sources which are common indoor lights and most challenging of all – the sun. 


Easier Calibration and Development

Accurately recording and calculating phase differences in iToF sensors requires precise calibration, an extremely time-consuming process. To ease this, we have developed a proprietary method that makes Hyperlux ID sensors easier to calibrate and thus faster to set up.

To aid in development, onsemi has constructed an easy-to-use development kit that includes a baseboard, a sensor headboard and a laser board. The kit can be used both indoors and outdoors with a range of 0.5 – 30 meters. It can produce depth maps, 3D point clouds, phase-out and depth-out data from an image.

Lastly, by using spread-spectrum techniques many iToF (and other infrared-enabled devices) sensors can be used in the same system without worry of other device interference.


onsemi’s iToF Sensors Do More for Less

iToF sensors are excellent at making accurate 3D depth measurements, which have won them a solid place in industrial and commercial applications. With remarkable improvements in performance and design simplification, onsemi’s Hyperlux ID depth sensors open a new world of applications for iToF depth sensing.

Compared to iToF sensors on the market today, Hyperlux ID depth sensors work more effectively with objects in motion, outdoors and at greater distances. In addition, due to their novel design, Hyperlux ID depth sensors are more cost-effective, take up less board real estate and are easier to work with.

The Hyperlux ID family of depth sensors presently consists of two products: the AF0130 and AF0131. The AF0130 includes built-in depth processing while the AF0131 does not, for customers who prefer to use their own original algorithms.

Learn more about Hyperlux ID iToF depth sensors


Additional Resources

White paper: Overcoming Challenges through Indirect Time-of-Flight Advancements

Video: Advancements with Indirect Time-of-Flight Depth Sensing from Hyperlux ID


--


Author Bio

Name: Steven Harris, Sr. Director of Marketing, Industrial and Commercial Sensing Division, onsemi

Steve Harris is the senior director of marketing within the Industrial and Commercial Sensing Division at onsemi. He joined Aptina in June 2012 where he was the product line manager for the security image sensor product line. During his time as the Product Line Manager for security, he oversaw a 3x growth in revenue, achieving number one in market share. After the onsemi acquisition of Aptina, he transitioned into the Automotive Solutions Division as the ecosystem development manager.

Featured

Hyperlux

onsemi has developed a new 2.1 µm super-exposure pixel image sensor family - Hyperlux, with a unique set of features that cater to both sensing and viewing camera applications. Hyperlux sensors range from 3 Megapixel (MP), 8MP and higher, capable of capturing unmatched 150 dB high dynamic range (HDR) images with 120 dB single exposure flicker free range. The Hyperlux family keeps all signal-to-noise ratio (SNR) transitions at 30 dB and above, even at high temperatures (up to +100°C junction). In low light conditions, these sensors outperform their counterparts with same sized pixel across extreme temperature conditions. This unique sensor family also boasts the lowest power consumption in the smallest form factor enabling an efficient camera design.

Machine Vision

Machine Vision is transforming industrial automation by enabling intelligent visual inspection, measurement, and decision-making across diverse sectors. As industries embrace digital transformation, machine vision systems are becoming essential for enhancing productivity, quality, and operational efficiency. These systems combine high-performance image sensors, advanced optics, and AI-powered processing to capture and analyze visual data in real time. From identifying defects in manufacturing lines to guiding robotic arms in assembly, machine vision ensures precision and consistency.

Driven by innovations in CMOS sensor technology, global shutter architectures, and AI-based image processing, machine vision systems now offer superior low-light performance, high dynamic range, and ultra-fast frame rates. onsemi’s portfolio, including the XGS, PYTHON, and Hyperlux sensor families, delivers scalable, power-efficient solutions tailored for both high-resolution and high-speed applications.

The integration of extended vision technologies like LiDAR, iToF and SWIR further expands machine vision’s capabilities, enabling accurate 3D mapping and object detection in dynamic environments. These advancements are pivotal for smart factories, autonomous robotics, and next-generation quality control systems.

Smart and Mobile Robotics

Smart robots—from robotic arms to autonomous delivery units and humanoids—are transforming industries with advanced sensing, AI, and intelligent algorithms. Unlike traditional robots, they perceive their surroundings, avoid obstacles, and collaborate seamlessly with humans and machines.

These mobile, connected systems handle tasks like transporting loads and performing repetitive operations, often powered by 12–48 V batteries. Their ability to work safely and efficiently alongside people boosts productivity and frees human workers for higher-value tasks.

onsemi simplifies robotic development with intelligent power and sensing solutions. onsemi portfolio includes high-resolution imaging, robust motor control, and compact, efficient battery charging—built on decades of automotive-grade reliability. With onsemi, your robots are ready to adapt, perform, and thrive in even the harshest industrial environments.

AF0130
iToF Depth Sensor, 1.2MP, Global Shutter, Hyperlux™ ID